{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Modifying PowerPacT H & J frame rotary handles for locking in the ON position
Issue:
Direct mounted rotary handle for S29337 for PowerPact H and J breaker: Is there a way to lock in the ON position?

Product Line:
Circuit Breakers

Resolution:
The direct mounted rotary handle S29337 is shipped to allow the breaker to be locked in the OFF position. If an application is required in which the rotary handle needs to be locked in the ON position, there is a method to do this. Watch the below video for a demonstration of how this is done.

Schneider Electric Canada