{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
TeSys U Single Phase Reversing
Issue:
Can the TeSys U be used on a single phase reversing motor?

Product Line:
TeSys U Starters - GIC Product

Environment:
US Product

Cause:
Product characteristics

Resolution:
The LUCC module is not considered compatible with the reversing modules. This is because of the way the reversing module reverses the motor leads. The TeSys U should not be used for single phase reversing loads.

Schneider Electric Canada