{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can we use any color cap with 9001KP** pilot lights?
Issue:
Choosing color caps for 9001KP pilot lights

Product Line:
9001 Harmony 30mm Push Buttons

Environment:
Push buttons and Operator Interface

Resolution:
Yes, it is possible
*Add 9001 in front to order separately
**If LED light modules are used, then the lens cap should match the color of the LED. Use yellow LED with an amber lens. See attached.

Schneider Electric Canada

Attachment(s)
ColorCaps.bmp [299.79 KB]