{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What ION7550/ION7650 firmware downloads are available and what changed?
Issue
Where can I download ION7550/ION7650 firmware and what was updated?

Product Line
ION7550/ION7650

Environment
Firmware Download Links

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


The table below lists the current and past firmware versions with associated downloads and What's New? document links:

Note: determine the hardware version of the meter from meter serial number, e.g. if the meter serial number is MW-1109A055-01, then its hardware version is -01, in this meter example firmware could be updated til v375.

Firmware VersionION7650 Firmware*ION7550 Firmware*What's New? DocumentNotesRelease Date
V415DownloadDownload
RTU**: Download
DetailsOnly compatible with -05 hardwareMay 2019
V411DownloadDownloadSee BelowOnly compatible with -05 hardwareJuly 2018
V410DownloadDownloadDetailsOnly compatible with -05 hardwareMarch 2017
V401DownloadNot AvailableDetailsOnly compatible with -05 hardwareMarch 2016
V400DownloadNot AvailableDetailsOnly compatible with -05 hardwareFeb 2015
V375DownloadDownloadSee BelowUse for -04 and older hardwareJuly 2018
V374DownloadNot AvailableDetailsMarch 2016
V373DownloadDownloadDetailsDec 2014
V371DownloadDownloadSee BelowJune 2012
V366DownloadDownloadSee BelowFeb 2012
V360Not AvailableDownloadDetails
V355Not AvailableNot AvailableDetails
V350Not AvailableNot AvailableDetails
V331Not AvailableNot AvailableSee Below
V330Not AvailableNot AvailableDetails
V321Not AvailableNot AvailableDetails

* Older versions with 'Not Available' status may be requested from Technical Support if required.
** RTU stands for Remote Terminal Unit

Additional descriptions for firmware versions are as follows:

V415
This firmware release adds a number of security enhancements to your meter such as the closing if unused ports, changing port assignments and tracking security events can help minimize the possibility of unauthorized intrusion.
V411/375
No new features.
V410​
This firmware release supports EN50160:2010 (Edition 4) and IEC 61000 4-30 Edition 3. EN50160 is a European standard that defines the voltage characteristics of the electricity supplied by public distribution systems. The latest firmware version for this meter now supports the EN50160:2010 (Edition 4) standard. The IEC 61000-4-30 (4-30) standard defines methods for measurement and interpretation of power quality parameters in 50/60 Hz AC power supply systems. The standard describes measurement methods for relevant parameters to obtain reliable, repeatable and comparable results using any compliant meter.
V400
V400 is a general firmware release that adds support for new metering hardware. In addition this firmware release reduces the 7x50e and 7x50s variants into one allowing for IEC61850 and10Meg of logging memory to occur upon the same device. V400 adds compatibility for the -05 hardware revision option. This can be found as the last two digits of a meters serial number. V400 will NOT be compatible with previous versions of hardware ( -04 or earlier). In addition previous firmware revisions (pre V400) will not be compatible with the -05 hardware. We have consolidated the e (IEC61850) and s (standard) variants into one release. This means ALL devices ordered with V400 will now contain IEC61850 functionality as well as contain the 10M logging memory. Both features can be implemented in frameworks simultaneously. NOTE: To support the new features in v400, download the latest version of ION Setup from the website.
V401/374
*The V374s version is the standard version. *The V374e version is for IEC61850 protocol support. This firmware is for the older hardware platform (RevA, if you like). The equivalent firmware for the RevB hardware platform is V401.
V373​
Firmware V373 is a general firmware release that adds support for the following features: (1) Access to more voltage data (2) Enhanced interharmonic distortion calculation (3) Display module enhancements (4) initial release of the PowerLogic Remote Display and also includes security enhancements. NOTE: For more detailed information about any of these features, please find the document entitled "What’s new in ION7550/ION7650 v373" (7EN12-0276-00). In preparation for upgrading your meter's firmware please download the latest firmware version (.upg file) and the appropriate Meter Template (.dcf file). Note that releases of Meter Template files often do not keep pace with firmware releases so do not be concerned if the firmware version number in the label of latest available template file is not as high as the version number of the firmware file. The main thing is to get the latest available file for each of firmware and template. ION Setup (freeware utility) is the recommended tool for the firmware upgrade process. See the Upgrading ION Device Firmware technical note for complete details.
Important Notes: *Generally, two versions of firmware are available for the ION7x50 devices: VXXXe with IEC 61850 implementation, and; VXXXs without IEC 61850 implementation. *IEC61850 is supported with the consequence of a reduction of the available logging memory. If you upgrade a 10MB meter to use IEC 61850 firmware, the meter’s logging memory will be reduced to 5MB. If the meter is subsequently loaded with non-IEC 61850 firmware, the meter’s original logging memory will be restored.

V371​
Firmware V371 is a general firmware release that adds support for the initial release of the PowerLogic Remote Display and also includes security enhancements. In preparation for upgrading your meter's firmware please download the latest firmware version (.upg file) and the appropriate Meter Template (.dcf file). ION Setup (freeware utility) is the recommended tool for the firmware upgrade process. See the Upgrading ION Device Firmware technical note for complete details.
Important Notes: *Two versions of firmware are available below namely: V371e with IEC 61850 implementation, and;V371s without IEC 61850 implementation. *IEC61850 is supported with the consequence of a reduction of the available logging memory. If you upgrade a 10MB meter to use IEC 61850 firmware (7650V360e), the meter’s logging memory will be reduced to 5MB. If the meter is subsequently loaded with non-IEC 61850 firmware (7650V360s), the meter’s original logging memory will be restored.
V366
Firmware version 366 (V366) for the ION7x50 adds Modbus mastering over TCP support for up to 10 connections. This is in addition to the 8 available Ethernet connections and is also in addition to the Modbus master functionality in both serial ports. This release also includes various communications bug fixes. When upgrading your meter's firmware please download the latest firmware version (.upg file) and the equivalent Meter Template (.dcf file). You can upgrade meter firmware using ION Setup or ION Enterprise. See the Upgrading ION Device Firmware technical note for complete details
Important Notes from V360 (applicable to V366): * Two versions of V360 firmware are available below: with IEC 61850 implementation (7x50V360e) and without IEC 61850 implementation (7x50V360s). * IEC 61850 can only be purchased on 5MB meters, not 10MB meters. If you upgrade a 10MB meter to use IEC 61850 firmware (7x50V360e), the meter’s logging memory will be reduced to 5MB. If the meter is subsequently loaded with non-IEC 61850 firmware (7x50V360s), the meter’s original logging memory will be restored.* The non IEC 61850 firmware version (7x50V360s) still has new features available, such as COMTRADE waveform recording.* To find ICD files related to the IEC61850 implementation on ION7x50 meters, search the keyword icd on any schneider-electric.xxx site
V360
Firmware version 360 (v360) for the ION7550/ION7650 adds IEC 61850 server functionality. This includes FTP support and the ability to save waveform data in COMTRADE format.
V355
Firmware version 355 (v355) and factory template 7550/7650_v355_FACPQ_V3.4.0.0.0 for the ION7550 / ION7650 adds International Electrotechnical Commission (IEC) 61000-4-30 Class A Edition 2 standard compliance for the ION7550 / ION7650 and the ability to configure the event priority value for digital input state change events.
V350
Firmware version 350 (v350) for the ION7550 / ION7650 adds a number of new features as well as support for the new Communications Card.
New features
  • Disturbance Direction Detection capabilities are now available.
  • Localization options have been added to the meter, including:
    • the ability to set the language of the front panel display to English, Spanish, French or Russian.
    • the option to customized IEEE/IEC convention settings.
  • Setpoint learning functionality has been added.
  • The meter can function as a Modbus gateway, forwarding Modbus packets from a master through the meter to downstream serial devices.
  • Trending and Forecasting functionality has been added.
  • The meter can now communicate selected values over the Ethernet via SNMP.
  • Support for a new communications card has been added.
  • A default IP Address has been added. For more information on these features, see the relevant sections in this document.
Other changes
  • Power Availability has been removed from the default template.
  • V4, I4, I5 waveform recorders have been removed from the default template.
  • Thermal Demand has been removed from the default template.
V331​
Firmware version 331 (v331) for the ION7550/ION7650 meter improves Class A compliance with the IEC 61000-4-30 (2003 - 1st Edition), or “4-30” power quality standard. Compliance improvements included are Class A Flicker with no exceptions
V330
Firmware version 330 (v330) for the ION7550 / ION7650 meter supports Class A compliance with the IEC 61000‐4‐30 (2003 ‐ 1st Edition), or “4‐30” power quality standard.
V321
Firmware version 321 features enhanced Modbus Mastering with four ION modules new to the ION 7550 /ION 7650 platform. The Modbus Master Device and Modbus Master Mapping modules work together to offer improved setup of Modbus read functionality. The Averaging module provides simple averaging and easily links with other Modbus modules. The Modbus Master Options module allows multiple serial connections to different loops of Modbus devices.
Advanced meter security provides an additional layer of security, allowing you to configure up to 16 users, each with unique access rights to the meter. Access rights consist of different security levels, permitting different users to read values, perform resets, time sync the meter clock, or configure meter settings.

Schneider Electric Canada