{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to control SR3NET01BD Modbus TCP device over Ethernet

Issue:
Zelio smart relay SR3NET01BD Modbus TCP control over Ethernet demonstration

Product Line:
Relays and Timers

Environment:
All Products

Cause:
Product Features

Resolution:
Following FAQ will introduce the basic setting and functionality for the SR3NET01BD Ethernet communication module.
A sample demo program has been built. A "word to bit" conversion function block is used to realize the function.

For an explanation of bit to word conversion in ZelioSoft please refer to our FAQ FA323130.

The following video demonstrates controlling a Zelio Smart Relay via Modbus TCP Over Ethernet:

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: