{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many auxiliary devices (Control Power Transformer or Voltage Transformer) can be placed in a structure of Square D Arc Resistant MasterClad Switchgear?
Issue:
Identify the amount of auxiliary devices that can be installed in Square D MasterClad Switchgears

Product Line:
Air-Insulated Switchgear

Environment:
MasterClad MV Switchgear

Resolution:
Two auxiliary devices (CPT – max 15kVA or VT) can be mounted in full height structure with no breakers.  One auxiliary device (CPT – max 15kVA or VT) can be mounted in a structure above or below a breaker (max 2000A).

Schneider Electric Canada