{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the end cap part number for I Line Busway part number AP308 ?
Issue:
What is the end cap part number for I Line Busway part number AP308 ? Can existing I Line 2 Busway end cap be used ?

Product Line:
I Line 1 Busway

Environment:
Maintenance

Cause:
Installation

Resolution:
The ACP5EC end closure will fit the AP308 Busway as well as the old 800A Copper CP308 Busway and the 1000A AP Busway with 4.75" width corrugated construction

Schneider Electric Canada