{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Will a Powerstyle switchboard with an I-line LA frame 400A existing breaker, accept a 400A Powerpact L breaker?

Issue:
Can you replace a legacy LA or LH I-line breaker with a Powerpact L frame breaker in a switchboard?

Product Line:
circuit breaker

Environment:
I-line, Switchboard, Powerstyle switchboard

Resolution:
Yes, as long as they are replacing an existing LA or LH  I-line constructed breaker, a Powerpact 400A L frame breaker will fit. Will need to verify before ordering. This is not true for Powerpact breakers above 400A. That will require an assessment.

Schneider Electric Canada