Search FAQs
AGS stops generator ~15 minutes after starting
Issue:
Generator only turns on for 15 mins without fully charging my batteries.
Product Line:
Conext Automatic Generator Started
Environment:
Inverter system with generator backup
Cause:
AGS Stop triggers are not set to desired configuration. Either the StopV trigger or the StopAbsorb are selected.
Resolution:
If the StopV trigger is enabled, make sure the voltage selected is not close to the Start Voltage.
When a full battery charge cycle is desired with the generator make sure to select StopFloat trigger instead of StopAbsorb. StopFloat will stop the generator at the end of the Absorption Stage (end of charging cycle) while StopAbsorb will stop generator at the end of the Bulk Stage (first charging stage).
Generator only turns on for 15 mins without fully charging my batteries.
Product Line:
Conext Automatic Generator Started
Environment:
Inverter system with generator backup
Cause:
AGS Stop triggers are not set to desired configuration. Either the StopV trigger or the StopAbsorb are selected.
Resolution:
If the StopV trigger is enabled, make sure the voltage selected is not close to the Start Voltage.
When a full battery charge cycle is desired with the generator make sure to select StopFloat trigger instead of StopAbsorb. StopFloat will stop the generator at the end of the Absorption Stage (end of charging cycle) while StopAbsorb will stop generator at the end of the Bulk Stage (first charging stage).
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: