{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I lower the amount of amps I can pull from my AC input?

Issue:
I want to limit the amount of amps I can draw from my AC input.

Product Line:
Conext SW/XW systems

Environment:
Conext SW/XW system with generator backup.

Cause:
Generator or AC input source has a current limit lower than what the inverter can handle, need to make sure it is not overloaded.

Resolution:
Go to the Inverter's menu Advanced Settings > AC settings, change the AC breaker size to the maximum you want the inverter to pull from your AC input. This will limit the inverter's pull and prevent any overload possible from your input.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: