{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Harmonized Tariff Code for ION Meters?
Issue:
Customer may need a Harmonized Tariff Code to ship ION Meters internationally

Product Line:
ION6200, ION7650, ION7550, ION8650

Environment:
International Shipping

Cause:
Harmonized Tariff codes are used to classify and define internationally traded goods. In most cases, to import or export a product internationally, the traded good must be assigned an HTS code that corresponds with the Harmonized Tariff Schedule of the country of import.

Resolution:
The Harmonized Tariff Code for ION Products is 9030.84

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.