{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do I need an SCP or Combox in my Conext SW/XW system?
Issue:
Do I need an SCP or Combox in my Conext SW/XW system?

Product Line:
Conext SW/XW+ inverters & Accessories

Environment:
New Conext SW/XW installation/setup

Cause:
New system installation without available System Control Panel or combox.

Resolution:
Although the inverters do not require a System Control Panel or Combox during startup you need one of these two units to change the settings from the default values. Having an SCP or Combox is also very helpful for monitoring and troubleshooting the system.
The default values on Inverters can be found in their respective Owner's Manual which can be found on our website.
www.sesolar.com

Schneider Electric Canada