{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the term interlock mean when referring to pushbuttons?
Issue:
What does interlock mean and what line of pushbuttons do we offer that are interlocked?

Product Line:
30 mm / 22 mm Pushbuttons and Operators

Environment:
9001K, 90010SK, XB4, XB5 push buttons

Resolution:
When two push buttons are interlocked, only one button can be pushed at a time. We have interlock mechanism available on the Class 9001 pushbuttons. The interlock mechanism is not available on the XB4/XB5 units.

Schneider Electric Canada