{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a model 6 or Model 5 MCC 150A branch feeder bucket?
Issue:
Is there a 150A branch feeder bucket available for a Model 5 or Model 6 Motor Control Center?

Product Line:
Motor Control Center

Environment:
Model 5 or Model 6

Cause:
Repair part needed or an addition required

Resolution:
Suggested the 8998SBF150 or the 8998HBF150. The 8998SBF150 is a 12" bucket with a vertically mounted breaker. The 8998HBF150 is a 6" bucket with a horizontally mounted breaker. Both buckets are rated 480V, Nema 12, at 100KAIC. If the MCC is a Model 5 please order the midshelf part number 80450-865-50.

Schneider Electric Canada