{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an enclosure for the 2510FR1 and 2510FR2 with two hubs?
Issue:
Manual starters 2510FR1 and a 2510FR2 enclosures

Product Line:
Fractional Horsepower Manual Starters

Environment:
NEMA Contactors and Starters

Resolution:
Enclosure of a 2510FR1 is rated NEMA 3R, 7 and 9. It is designed to have a hub only at the bottom because of the rating of the enclosure.

Schneider Electric Canada