{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the SASFB type subfeed breaker kits be installed on the I-line distribution Speed D Switchboards?

Issue:
Are subfeed breaker kits available for the I-line distribution Speed D SWBD's?

Product Line:
Switchboards

Environment:
Speed D

Resolution:
No. The SASFB kits can only be used on the Speed D boards that have the NQ interiors installed. However, There is room for 1 - LA breaker to be installed with 125A - 400A ratings.

Schneider Electric Canada