{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a 24VAC coil available for the Size 4 - 7 8536/8502?
Issue:
Looking for a 24V coil on a Size 4 - 7 Type S NEMA Contactor

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
No, 24VAC coil are only available for Size 00 - 3, and 24VDC coils are not available for NEMA starters.

Schneider Electric Canada