{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum clearance requirement for MPZ/B transformer?
Issue:
Clearance for MPZ/B transformers



Product Line:
Transformers


Environment:
Mini power zone


Cause:
Location Clarification


Resolution:
The MPZ/B has a clearance requirement of at least 12" or 13" from front, top, bottom, and sides to any obstruction.  The clearance requirement is shown on the NamePlate.  The clearances for such Transformers are established per UL mandated alcove testing procedures, in which such tests are conducted in a prefabricated alcove testing space with those required clearance dimensions.  The testing, when done and passed, obtain UL approval for that catalog number of Transformer, and the required clearances printed on the NamePlate are a reflection of that UL mandated testing regimen.  The clearances presume to a achieve adequate proper airspace to cool the Transformer properly, so we require them per UL mandates.

Schneider Electric Canada