Search FAQs
Are the GS2 and LK4 disconnect handles defeatable?
Issue:
Checking if the GS2 and LK4 disconnect handles are defeatable
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
LK4 Non Fusible and GS2 Fusible Disconnect Switches
Resolution:
Yes. With a tool, the door interlock can be bypassed. This allows the door to be opened when the switch is in the ON position.
Checking if the GS2 and LK4 disconnect handles are defeatable
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
LK4 Non Fusible and GS2 Fusible Disconnect Switches
Resolution:
Yes. With a tool, the door interlock can be bypassed. This allows the door to be opened when the switch is in the ON position.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: