{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the pilot light light used on 8903LX lighting contactor?
Issue:
What is the pilot light light used on 8903LX lighting contactor?

Product Line:
Lighting Contactors

Environment:
Multipole Lighting Contactors, Type L and LX

Resolution:
9999SP28R is the pilot light used for electrically held. The same pilot light assembly can't be used for mechanically held because of coil clearing contact. Customer can use half of the snap switch that is not being utilize by the lighting contactor as a power source. Suggest to use 9001KP pilot light instead and wire it up themselves from the snap switch

Schneider Electric Canada