Search FAQs
What is the replacement DC coil for the 8501XD, 8501XDL, and 8501XUD relays
Issue:
DC coil for the 8501 relay needs to be replaced
Product Line:
Relays and Timers
Environment:
NEMA Style DC Relays
Resolution:
Please see list below and check first if the part number is still active as some may already be obsolete.
DC coil for the 8501 relay needs to be replaced
Product Line:
Relays and Timers
Environment:
NEMA Style DC Relays
Resolution:
Please see list below and check first if the part number is still active as some may already be obsolete.
Voltage | 8501XD | 8501XDL | 8501XUD |
6 VDC | 9998XD19 | 9998XDL19 | 9998XUD19 |
12 VDC | 9998XD28 | 9998XDL28 | 9998XUD28 |
18 VDC | 9998XD34 | 9998XDL34B | - |
24 VDC | 9998XD37 | 9998XDL37B | 9998XUD37 |
32 VDC | 9998XD40 | 9998XDL40B | - |
48 VDC | 9998XD46 | 9998XDL46B | 9998XUD46 |
64 VDC | 9998XD49 | 9998XDL49B | - |
72 VDC | 9998XD52 | 9998XDL52B | - |
90 VDC | 9998XD55 | 9998XDL55B | - |
115/125 VDC | 9998XD58 | 9998XDL58B | 9998XUD (125VDC) |
230/250 VDC | 9998XD67 | 9998XDL67B | 9998XUD67 |
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: