{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the enclosure features for the Arc resistant Model 6 MCC's (Motor Control Centers)?

Issue:
What are the enclosure features for the Arc resistant Model 6 MCC's?

Product Line:
Model 6 Arc Resistant Motor Control Centers

Environment:
Application

Cause:
Product Features

Resolution:
The attached Data Bulletin with the Model 6 Arc Resistant Rated Motor Control Center, is tested per the ANSI C37.20.7 guidelines, with the following enclosure features:

• UL 50E Type 1, 12, and 3R
• Exhaust type
— Roof flaps
— Plenum

Schneider Electric Canada

Attachment(s)

Model 6 Arc resistant  8998DB1301.pdfModel 6 Arc resistant 8998DB1301.pdf [48.45 KB]