{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is the magnet that holds the coil in the IEC Tesys F contactors replaceable?

Issue:
What is the part number of the E shaped metal part that holds the coil in the Tesys F Contactors?

Product Line:
IEC Tesys F Contactors

Environment:
IEC Tesys F Contactors sold and used in the United States

Resolution:
No. The part that holds the coil on the Tesys F contactor is not a replaceable part. If lost or damaged, you will have to replace the contactor.   This should come with the contactor not with the coil.

Schneider Electric Canada