Issue:
What are the Pressure setting or J Codes for 9013 pressure switch ?
Product Line:
Class 9013 Type FHG—Pumptrol Compressor Pressure Switch
Environment:
Commercial Pressure Switches
Resolution:
Below are the standard Pressure Code (fixed differential) for Class 9013 Type FHG pressure switches.
What are the Pressure setting or J Codes for 9013 pressure switch ?
Product Line:
Class 9013 Type FHG—Pumptrol Compressor Pressure Switch
Environment:
Commercial Pressure Switches
Resolution:
Below are the standard Pressure Code (fixed differential) for Class 9013 Type FHG pressure switches.
Off at... | Code |
80 psi | J43 |
100 psi | J27 |
110 psi | J37 |
115 psi | J38 |
120 psi | J69 |
125 psi | J52 |
135 psi | J39 |
140 psi | J68 |
155 psi | J40 |
150 psi | J55 |
175 psi | J59 |
Specify other pressure | J99 |
(minimum order quantity is 4 pieces) J99 |