{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a flush or surface mount stainless steel trim available for an NQ or NF panelboard? What is the NEMA enclosure rating?
Issue:
Stainless steel trim for panelboard enclosure
Product Line:
Panelboard
Environment:
NQ/NF Type Panelboard
Cause:
Product feature and application clarification
Resolution:
Yes, a stainless steel version of the Mono-Flat front is available for either flush or surface mount NEMA 1 enclosures.  A surface-hinged or flush-hinged trim is also available.  Any of these can be configured using the panelboard product selector.    The enclosure is rated NEMA 1.  It is not rated NEMA 4/4X.  A flush mounted NEMA 4/4X enclosure is not available.  We do offer surface mount NEMA 4/4X enclosures, and there are versions available using stainless steel (standard 304 or optional 316) or fiberglass.

Schneider Electric Canada