{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are all Tesys F DC coils have built-in surge suppression?
Issue:
Does the 3 and 4 pole Tesys F DC coil have built-in surge suppression?

Product Line:
IEC Tesys F Contactors, F115–F330, F400–F630, F780, F1400–F2100

Environment:
Contactors and Starters-IEC

Resolution:
Only 3-pole DC contactors coils are fitted with built-in surge suppression as standard.

Schneider Electric Canada