Issue:
Does the 2p H frame breaker have an optional terminal cover?
Product Line:
Circuit Breakers
Resolution:
The answer depends on the following:
1. Is it a 2 pole HD, HG, HJ, or HL breaker?
Does the 2p H frame breaker have an optional terminal cover?
Product Line:
Circuit Breakers
Resolution:
The answer depends on the following:
1. Is it a 2 pole HD, HG, HJ, or HL breaker?
- If HD or HG, there are no optional terminal covers for the 2 pole versions.
- If HJ or HL, go to the next question.
- If HJA or HLA, the terminal shield is part number HDTC. Quantity of 1 for the load end.
- If HJL or HLL, the 15 - 60 A terminal shield is part number S37446. Quantity of 2, one for each end.
- If HJL or HLL, the 70 - 150 A terminal shield is part number S37447. Quantity of 2, one for each end.
Released for:Schneider Electric Canada