{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an ELM module be used on a 208 or a 120 V system?
Issue:
What is the minimum voltage system an ELM module can be applied on?

Product Line:
Circuit Breakers

Resolution:
The ELM150HD and ELM250JD may be applied on systems only between 240 and 600 Vac. The electronics are powered from bus voltage and the voltage must be in this range.

Schneider Electric Canada

Attachment(s)
ELM 0611HO0901.pdf [202.99 KB]
ELM Instr 48041-089-01 2010.pdf [6.17 MB]