Search FAQs
What is the DC replacement coil for an LC1F185 and LC1F225?
Issue:
Is there a 220Vdc replacement coil for an LC1F185 and LC1F225 ?
Product Line:
IEC Tesys F Contactors, F185, F225
Environment:
IEC Tesys F Contactors sold and used in the United States
Resolution:
LX4FG replacement coils are the standard coils when a voltage code is added to the part number. The LX4 coils can also be used
on previous TeSys F devices. Below list the DC replacement coil for LC1F185 and LC1F225.
LX4FG024 24Vdc
LX4FG035 36Vdc
LX4FG048 48Vdc
LX4FG060 60Vdc
LX4FG070 72Vdc
LX4FG110 110Vdc
LX4FG125 125Vdc
LX4FG220 220Vdc
LX4FG250 250Vdc
LX4FG440 440Vdc
Is there a 220Vdc replacement coil for an LC1F185 and LC1F225 ?
Product Line:
IEC Tesys F Contactors, F185, F225
Environment:
IEC Tesys F Contactors sold and used in the United States
Resolution:
LX4FG replacement coils are the standard coils when a voltage code is added to the part number. The LX4 coils can also be used
on previous TeSys F devices. Below list the DC replacement coil for LC1F185 and LC1F225.
LX4FG024 24Vdc
LX4FG035 36Vdc
LX4FG048 48Vdc
LX4FG060 60Vdc
LX4FG070 72Vdc
LX4FG110 110Vdc
LX4FG125 125Vdc
LX4FG220 220Vdc
LX4FG250 250Vdc
LX4FG440 440Vdc
Released for:Schneider Electric Canada
Explore more
Product:
Range:
Explore more
Product:
Range: