Issue:
9001BW pendant stations may have broken or defective push button or contacts that will need replacement
Product Line:
Pendant Stations
Environment:
Type BW Pendant Stations
Resolution:
The replacement interior includes the contacts and buttons, and some also includes inserts. The contacts and buttons not replaceable as separate components.
9001BW pendant stations may have broken or defective push button or contacts that will need replacement
Product Line:
Pendant Stations
Environment:
Type BW Pendant Stations
Resolution:
The replacement interior includes the contacts and buttons, and some also includes inserts. The contacts and buttons not replaceable as separate components.
Pendant Station | Replacement interior | Legend Insert | Type of Contact |
9001BW92Y / 9001BW92B / 9001BW92R | 9001BOC368 | Up-Down | Momentary |
9001BW93Y / 9001BW93B / 9001BW93R | 9001BOC368 | Forward-Reverse | Momentary |
9001BW94Y / 9001BW94B / 9001BW94R | 9001BOC358 | On-Off | Maintained |
9001BW95Y / 9001BW95B / 9001BW95R | 9001BOC359 | Start-Stop | Momentary |
9001BW96Y / 9001BW96B / 9001BW96R | 9001BOC358 | Start-Stop | Maintained |
9001BW97Y / 9001BW97B / 9001BW97R | 9001BOC359 | On-Off | Maintained |
9001BW98Y / 9001BW98B | none | Up-Down | Momentary |
9007BW90YU / 9007BW90BU / 9007BW90RU | 9001BOC366 | none | Momentary |
9007BW91YU / 9007BW91BU / 9007BW91RU | 9001BOC359 | none | Momentary |
9007BW94YU / 9007BW94BU / 9007BW94RU | 9001BOC358 | none | Maintained |
9001BW100YU / 9001BW100BU / 9001BW100RU | 9001BOC367 | none | Momentary |
9001BW102Y / 9001BW102B / 9001BW102R | 9001BOC367 | Up-Down | Momentary |
Released for:Schneider Electric Canada
Issue:
9001BW pendant stations may have broken or defective push button or contacts that will need replacement
Product Line:
Pendant Stations
Environment:
Type BW Pendant Stations
Resolution:
The replacement interior includes the contacts and buttons, and some also includes inserts. The contacts and buttons not replaceable as separate components.
9001BW pendant stations may have broken or defective push button or contacts that will need replacement
Product Line:
Pendant Stations
Environment:
Type BW Pendant Stations
Resolution:
The replacement interior includes the contacts and buttons, and some also includes inserts. The contacts and buttons not replaceable as separate components.
Pendant Station | Replacement interior | Legend Insert | Type of Contact |
9001BW92Y / 9001BW92B / 9001BW92R | 9001BOC368 | Up-Down | Momentary |
9001BW93Y / 9001BW93B / 9001BW93R | 9001BOC368 | Forward-Reverse | Momentary |
9001BW94Y / 9001BW94B / 9001BW94R | 9001BOC358 | On-Off | Maintained |
9001BW95Y / 9001BW95B / 9001BW95R | 9001BOC359 | Start-Stop | Momentary |
9001BW96Y / 9001BW96B / 9001BW96R | 9001BOC358 | Start-Stop | Maintained |
9001BW97Y / 9001BW97B / 9001BW97R | 9001BOC359 | On-Off | Maintained |
9001BW98Y / 9001BW98B | none | Up-Down | Momentary |
9007BW90YU / 9007BW90BU / 9007BW90RU | 9001BOC366 | none | Momentary |
9007BW91YU / 9007BW91BU / 9007BW91RU | 9001BOC359 | none | Momentary |
9007BW94YU / 9007BW94BU / 9007BW94RU | 9001BOC358 | none | Maintained |
9001BW100YU / 9001BW100BU / 9001BW100RU | 9001BOC367 | none | Momentary |
9001BW102Y / 9001BW102B / 9001BW102R | 9001BOC367 | Up-Down | Momentary |
Released for:Schneider Electric Canada