Issue:
Can the ELM be set to have a 100mA ground fault pick up?
Product Line:
Circuit Breaker Accessory
Resolution:
You can set the module to 30 mA, 100 mA, 300 mA, 1A, or 3A. These settings are digital, not analog, so settings between those are not available.
Can the ELM be set to have a 100mA ground fault pick up?
Product Line:
Circuit Breaker Accessory
Resolution:
You can set the module to 30 mA, 100 mA, 300 mA, 1A, or 3A. These settings are digital, not analog, so settings between those are not available.
Released for:Schneider Electric Canada