{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cleaning up UMAC conversion errors with Unity or Control Expert
Issue:
After using the UMAC tool to convert a Unity Quantum project to M580 some conversion errors appear.

Product line:
Modicon M580, Unity Pro, Control Expert

Resolution:
After the converted project is opened with Unity pro, any errors will show up in the output window. Double clicking on these errors will take the programmer to the location of the errors so that they may be corrected. Most errors from the UMAC conversion are just informative that can be commented out.

Schneider Electric Canada