{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the Phaseo ABL Power Supplies have a Current Limiting feature?
Issue:
Customer asking if Current Limit is a feature for the ABL8 power supply.

Product line:
Power supplies for industrial use

Environment:
ABL7RP ABL8REM Optimum

Resolution:
All the Optimum range of Phaseo power supplies have protection devices to ensure optimum performance of the automation system with an automatic reset mode on elimination of the fault.
In the event of an overload or short-circuit, the integrated protection interrupts the current supply before the output voltage drops below 19 Vdc. The protection device resets itself automatically on elimination of the fault, which avoids having to take any action or change a fuse.

Output  protection type
Against overload, protection technology: 1.1 x In
Against overvoltage, protection technology: tripping if U > 1.5 x Un
Against short-circuits, protection technology: automatic reset
Against undervoltage, protection technology: tripping if U < 0.8 x Un

Schneider Electric Canada