{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many Administrators are allowed for the XB5S2B2L2 biometric switch?
Issue:
Customer wants to know the maximum allowed number of Administrators allowed on the Biometric switch.

Product line:
XB5 XB5S1 XB5S2 biometric

Cause:
No reference to limits in the manuals.

Resolution:
The total number of fingerprints is limited to 200.  This is a total of both Users and Administrators.

Schneider Electric Canada