{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Zelio smart relay USB cable for Windows 10 and Windows 8.1 system?

Issue:
Zelio smart relay USB cable for Windows 10 and Windows 8.1 system

Product Line:
Relays and Timers

Environment:
Zelio smart relay

Cause:
Zelio smart relay USB cable for Windows 10 and Windows 8.1 system?

Resolution:
A change was made to the USB cord used to connect to the SR2 and SR3 smart relays.  With this new change, a new driver was released as well.
Part number of the cable is still SR2USB01, but the new version of this cable have a marking of 'H2.0' on it.
A new USB cable driver will be needed. See following link for detail: https://www.se.com/ww/en/download/document/DriverSR2USB01_H2/

Note: new USB cable and driver are compatible with WIN7 as well.

Schneider Electric Canada