{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can Powerpact 500 Vdc breakers be 100% rated?
Issue:
Are 500 Vdc Powerpact breakers for ungrounded UPS systems rated for application at 100% of their rating?

Product Line:
Circuit Breakers

Resolution:
No, these breakers are standard 80% rated and are not available with 100% ratings.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top