{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Are The Available Shorting Links For The GS2 Fusible Switches?
Issue:
Need to convert GS2 fusible to non-fused disconnect

Product Line:
Operating Mechansms and Disconnect Switches

Environment:
GS2 Fusible Disconnect Switches

Resolution:
The part numbers are as follows:

For use on:

Shorting Links per Kit

Catalog No.

GS2, 60 A

3

GS1AU203

GS2, 100 A

3

GS1AU303

GS2, 200 A

3

GS1AU403

GS2, 400 A

3

GS1AU503

GS2, 600–800 A

3

GS1AU803

Schneider Electric Canada