{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the default IP address of a Tesys T with ethernet port (LTMRxxExx)
Issue:
How to find the default IP address of a Tesys T with ethernet port.

Product Line:
Tesys T
LTMR

Environment:
Motor management

Resolution:
The LTMR controller derives its default IP parameters from its MAC address (stored in the device’s
Ethernet MAC Address parameter). The MAC address is a unique identifier associated with the device’s
network interface card (NIC).

The default IP parameters are generated as follows:
- The first two byte values of the IP address are always 85.16
- The last two byte values of the IP address are derived from the last two bytes of the MAC address
- The default subnet masks are always 255.0.0.0
- The default gateway is the same as the device’s default IP address

For example, for a device with a hexadecimal MAC address of 0x000054EF1001, the last two bytes are
0x10 and 0x01. These hexadecimal values translate to decimal values of 16 and 01. The default IP
parameters for this MAC address are:
- IP address: 85.16.16.01
- Subnet mask: 255.0.0.0
- Gateway address: 85.16.16.01

Schneider Electric Canada