Issue:
Is there a replacement for a VK-9223-603-4-11 valve?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
A new VB-7XXX Series Valve would need to be ordered as well as a new Actuator for it. The MK-6821 original actuator for the VB-9223 valve has a 1" stroke and will not work with the VB-7XXX Series valve .
A new MK-6621 actuator can be used to replace existing MK-6821 Actuator and can be ordered with the VB-7XXX series valve with an assembly number VK-7223-613-4-11
Is there a replacement for a VK-9223-603-4-11 valve?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
A new VB-7XXX Series Valve would need to be ordered as well as a new Actuator for it. The MK-6821 original actuator for the VB-9223 valve has a 1" stroke and will not work with the VB-7XXX Series valve .
A new MK-6621 actuator can be used to replace existing MK-6821 Actuator and can be ordered with the VB-7XXX series valve with an assembly number VK-7223-613-4-11