{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the power consumption for the Powerpact B frame shunt trip (MX) and undervoltage release (MN)?

Issue:
Power consumption of shunt trip and undervoltage release for B-frame circuit breakers
Product Line:
Molded Case Circuit Breakers
Resolution:
See table below:

Characteristics

AC

DC

Rated voltage (V)

24, 48, 110–130,

208–240, 277,

380–415, 440–480

24, 48, 125, 250

Power requirements

MX

Pickup (< 50 ms)

< 6 VA

< 10 W

Seal-in

< 4 VA

< 1 W

MN

< 7 VA

< 2 W

Clearing time (ms)

< 50

< 50

Operating range

Up to 1.1xVn

Up to 1.1xVn

Schneider Electric Canada