{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where are the conduit knockouts located on the MD3304X and MD3604X motor disconnect switches?

Issue:
Knockouts for MD motor disconnects.

Product Line:
UL 508 Motor Disconnect Switches

Environment:
Type MD motor Disconnect Switches

Resolution:
Customer may choose where they want to drill their holes for conduit. Eight drill points are provided as a guide for drilling the conduit entry hole in the top, bottom, or sides. See attached instruction bulletin.

Schneider Electric Canada

Attachment(s)

MD3304X and MD3604X, Instruction Bulletin IS 536778.pdfMD3304X and MD3604X, Instruction Bulletin IS 536778.pdf [738.37 KB]