Issue
How to verify CM3000/CM4000 series meter KYZ operation?
Product Line
CM3000 series meter
CM4000 series meter
Environment
Modbus Tool, Register List
Cause
How to verify the CM3000/CM4000 series KYZ pulses are being sent.
Resolution
To verify if the KYZ pulses are being sent, you can read the I/O point registers.
For example, the CM4000T Standard output (S01) registers start at 4300.
- If your looking for the IO Point Label read the register Base +1, which is register 4301.
- If your looking for the Discrete Input On/Off Status read the register Base +25, which is register 4325.
- If your looking for the Count read the register Base + 26, which is register 4326.
By referring to the IO Point Label, Discrete Input ON/Off Status and the count, you can verify the KYZ pulse operation.
To find the CM3000 and CM4000 series meter registers, please refer to FA212657.
For a simple tool that can read Modbus register, please download Modbus Tester from FA180037.