{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the operating temperature of an 0453L0077GA00 damper actuator?
Issue:
Is there Literature showing the operating temperature of the 453X Series damper actuators

Product Line:
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
The ambient operating temperature for the actuator is 0 DEG to +120 DEG F (-17 DEG to + 49 DEG C)

Schneider Electric Canada

Attachment(s)
0453 Damper Actuators F-27028-3.pdf [111.58 KB]