{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: Where are the mains rating, bus bar rating, cover number, lug torque data, and short circuit current rating located on the QO and Homeline load centers?
Issue:
Locating the mains rating, bus bar rating, short circuit rating, wiring diagram, cover number, and lug torque specification on Square D™ QO™ and Homeline™ Load Centers.

Product Line:
QO and Homeline Load Centers

Resolution:
The maximum mains rating, bus bar rating, load center cover number, lug torque data, and short circuit current rating will be located on the box label of the load centers. The box label is approximately 2.5" wide x 8.5" long and is located on one of the inside side walls of the enclosure.

SEE BELOW SAMPLE VISUALS OF A BOX LABEL

Label display

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: