Issue:
What is the maximum length the offset can be for Busway Edge wise elbow with suffix OE?
Product Line:
I line II Busway
Environment:
Application
Cause:
Product Features
Resolution:
The minimum edgewise offset is 6" as noted. That may be increased in one inch increments. Once the offset reaches 22 inches, we apply two standard edgewise elbows unless there is a joint restriction - such as a wall or floor penetration. The maximum one piece edgewise offset is 48 inches so the range for a one piece OE is 6" - 48".
What is the maximum length the offset can be for Busway Edge wise elbow with suffix OE?
Product Line:
I line II Busway
Environment:
Application
Cause:
Product Features
Resolution:
The minimum edgewise offset is 6" as noted. That may be increased in one inch increments. Once the offset reaches 22 inches, we apply two standard edgewise elbows unless there is a joint restriction - such as a wall or floor penetration. The maximum one piece edgewise offset is 48 inches so the range for a one piece OE is 6" - 48".
Released for:Schneider Electric Canada