{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION9000 Communication Ports and Protocols
Issue
Supported communication ports and protocols on ION9000.

Product Line
ION9000

Environment
Communication port/protocol.

Cause
Communication ports and protocols available on ION9000.

Resolution
1. Ports
- RS-485 port(s): 2
- Ethernet port(s): 2x 10/100BASE-TX, RJ45 connector, CAT5/5e/6/6a cable

2. Protocols
- Serial port protocols (Modbus, ION, DNP3)
- Ethernet port protocols (Modbus/TCP, ION TCP, DNP3 TCP, DHCP, DNS, IPv4, IPv6, IEC 61850)
- Ethernet gateway

3. Other Features:
- Alarm notification via email
- HTTP/HTTPS web server with waveform viewer
- SNMP with custom MIB and traps for alarms
- SMTP email
- PTP and NTP time synchronization
- FTP file transfer

Schneider Electric Canada