{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the availability of a VL-500 Erie Boiler Boss Controller Box?

Issue:
Can the VL-500 still be ordered ?

Product Line:
Field Devices

Environment:
Maintenace

Cause:
Replacement

Resolution:
The VL500 Boiler Boss Zone zone control system provided control of up to five zone valves, a circulator and boiler control in a multi-zone hydronic heating system. Field selectable priority for zone 1 eliminates the need for additional relays to provide domestic hot water priority. Additional zones can be added.
Unfortunately it is no longer available , see attached .

Schneider Electric Canada

Attachment(s)

Erie Boiler Boss Cancelation PA.pdfErie Boiler Boss Cancelation PA.pdf [61.5 KB]