{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an LSIG main breaker I-line panelboard be ordered in an outdoor NEMA 3R enclosure?
Issue:
Application of Micrologic ground-fault capable main breaker in a NEMA 3R I-line panel

Product Line:
I-Line Panelboard

Environment:
I-line panelboards in NEMA 3R enclosures with ground-fault main breakers

Cause:
Product selector will not allow selection of LSIG main breaker for I-line panelboard in NEMA 3R enclosure

Resolution:
No.  Ground fault capable LSIG main breakers for I-Line panels are NOT available in NEMA 3R enclosures.  The GF feature requires a box extension for the Neutral CT assembly and NEMA 3R boxes cannot be extended.  Possible solutions are to switch to a NEMA 1 application or to use a remote main breaker in a separate enclosure with a Micrologic LSIG trip unit.

Schneider Electric Canada