Issue:
Instruction bulletin to get the component part numbers for the 8502SB* and 8536SB* devices
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES A and B Starters Class 8502/8536, using the melting alloy or solid starter overload relay.
File name 30072-013-22 using the solid state overload relay
File name 30072-013-09 using the melting alloy overload relay
Instruction bulletin to get the component part numbers for the 8502SB* and 8536SB* devices
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES A and B Starters Class 8502/8536, using the melting alloy or solid starter overload relay.
File name 30072-013-22 using the solid state overload relay
File name 30072-013-09 using the melting alloy overload relay