{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where Can I Get The Instruction Bulletin for the NEMA Size 5 8502/8536 Type SG Contactors and Starters?
Issue:
Instruction bulletin to get the component part numbers for the 8502SG* and 8536SG* devices

Product Line:
NEMA Contactors and Starters

Environment:
Class 8502/8536 Contactors and Starters

Resolution:
The attached files are for SERIES A and B Starters Class 8502/8536, 2 and 3 poles, using the melting alloy or solid starter overload relay.

File name 30072-013-47, 3-pole using the solid state overload relay Series A
File name 30072-013-18, 2 & 3 poles using the melting alloy overload relay, Series A
File name ​30072-013-103, 2 & 3 poles using the melting alloy overload relay, Series B

Schneider Electric Canada

Attachment(s)
30072-013-18.pdf [79.12 KB]
30072-013-103.pdf [323.75 KB]
30072-013-47.pdf [106.59 KB]